Other Parts Discussed in Thread: DRV8329, DRV8328, DRV8300, DRV8308, DRV8320, DRV8320R, DRV8323R, DRV8323, MOTORWARE
Hello,
I am finding BLDC motor controller and found the 8316 series.
Looks like good one but I have some questions.
1. I will use 24VDC 100W motor and Motor Winding RMS current is about 4A.
Is it working with 8316 series?
2. A similar system has a BEMF of 50 A peak.
Is it Ok?
3. I used BLDC_Int_Thermal_Clac...
Looks like Junction Temp is very high.
Is it Ok?
4. PCB Top/Bottom Layers Cu Thickness.
Do I have to use 2 oz of thickness?
Looks like can't calculate about 1 oz.
I'd appreciate it if you could give me an answer.
Thank you.