Other Parts Discussed in Thread: DRV8323
Hi
I am using Isolator to DRV8323 6X PWM Input INHx and INLx pins for isolate driver part with different power domain. I observed that there is 8ns delay between input and output pins and rise/fall time same as controller output.
The motor without isolator is running perfectly , with iso there are distortion in motor commutation, cause of that FETs are taking high amount of current to rotate the motor. there is no fault flag i can read from fault registers.
What could be the reason to not following the same commutation to the output ?
Isolator Specification :
Output Rise/Fall Time - tR/tF 2.5 ns
Typical SWITCHING SPECIFICATIONS -
Pulse Width PW 6.6 ns
Data Rate 150 Mbps Max
Propagation Delay tPHL, tPLH 8.7 ns
Sourcing Current - 4.4 mA @ 1 Mbps