Hi Expert,
Our customer would like to use DRV890X-q1 in a door control unit. Now they have some concern about its thermal performance. As shown in datasheet, the normal output current is 1A RMS. They will use two half bridge to driver a motor as H bridge. They would to evaluate the worst case. Now one DRV8912-Q1 drives 6 motor, which means all 12 channels are all used. The nominal output current is 1A RMS. What's the thermal performance of DRV8912-Q1? Or normally, for 1A RMS load current, what's the duty cycle do you recommend with 12CHs? It will be great if you can share related test report. Thanks.
BR,
Elec Cheng