I marked my previous question as closed too soon, the program still crashes 90% of the time when I try connecting the the Haptic Control Console to the DRV2625EVM-CT.
Do any of the other haptic motor eval kits have support for Windows 11?
When I attempted to use the DRV2625EVM-CT, the Haptic Control Console 1.6.0.2 crashes when I press 'connect'. I see from a different forum post that I would need Windows 7 to connect with DRV2625EVM-CT. Are there any other haptic driver eval kits which will actually work with the Haptic Control Console on Windows 11?