This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2625EVM-CT: Windows 11 supported haptic driver eval kit

Part Number: DRV2625EVM-CT

I marked my previous question as closed too soon, the program still crashes 90% of the time when I try connecting the the Haptic Control Console to the DRV2625EVM-CT.

Do any of the other haptic motor eval kits have support for Windows 11? 

When I attempted to use the DRV2625EVM-CT, the Haptic Control Console 1.6.0.2 crashes when I press 'connect'. I see from a different forum post that I would need Windows 7 to connect with DRV2625EVM-CT. Are there any other haptic driver eval kits which will actually work with the Haptic Control Console on Windows 11?