Part Number: DRV120
Hello,
I have a question regarding the maximum supply voltage of the DRV120. On the TI product page it is listed as 26V, in the datasheet on multiple occasions a supply voltage of 6-28V is mentioned. Yet, 28V is then listed in the same datasheet as the absolute maximum supply voltage, and the optimal supply voltage is given up to 26V. The data sheet then mentions that "Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability".
To my understanding this means that the maximum operating voltage is indeed 26V and not 28V. Or is this a typo and the absolute maximum rating should be higher than 28V ?
Kind regards