Part Number: DRV8432
hello, i have a question about the DRV8432 thermal calculation
the spec of DRV8432 shows it can output 2*7A continous and 2*12A peak.
but when i do the thermal calculation i found if i output 2*7A current, the Tj will be 311℃ which exceed a lot from the maximum Tj 150℃
below is the calculation of the thermal
- Tj= Ta+RθjA*Pd
- Pd=Imax^2*(Rds(on)high+ Rds(on)low)*2
- Imax=7A
- Rds(on)high=Rds(on)low=0.11Ω
- RθjA=13.3℃/W
- Ta=25℃
- Tj=25+13.3*21.56=311℃
if we want to keep the Tj below 150℃,and use two full bridge drive two BDC motor, the maximum current should not exceed 2*4.6A, this is miss match the output current with 2*7A
could you help me to answer my confuse and give me some advise about is it possible to use this IC to output 2*6.2A continous current
thanks a lot