Dear Specialists,
My customer is considering DRV10983 and has a question about programming voltage,
I would be grateful if you could advise.
---
I have a question about writing to the EEPROM of the motor driver IC DRV10983.
I am writing to the EEPROM of the DRV10983 using the MSP430 microcomputer.
In "8.3.5 Non-Volatile Memory" of the DRV10983 datasheet
The procedure for writing to EEPROM is described, but "4. Ensure that VCC is at or above 22 V."
When writing voltage of Vcc is less than 22V, what are the results?
I think that there are phenomena such as
・Writing is not performed
・The write has completely failed, and there is no change in the written contents in the EEPROM
・Although writing is executed, there is a possibility that writing failures such as missing bits may occur due to insufficient voltage.
But do you know how it behaves?
I am worried about whether the written contents in the EEPROM will be affected.
I'm worried about how the written contents in the EEPROM will be affected when the write voltage is insufficient.
---
I appreciate your great help in advance.
Best regards,
Shinichi