Hello,
1. Please check whether the schematic design of the accessories is reasonable?
2. The two DRV8860 are not connected to the load. Why is the FAULT pin not pulled down?
3. How to test the open circuit protection function?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
1. Please check whether the schematic design of the accessories is reasonable?
2. The two DRV8860 are not connected to the load. Why is the FAULT pin not pulled down?
3. How to test the open circuit protection function?
Hello,
You need a pull-up resistor on the nFAULT pins. It is an open-drain output. Recommend 10K.
See 8.3.3.2
For your schematic, I would toggle J4 (manual valve) and see if OLD detects on U10. Or disconnect the load on OUT4.
Here is another E2E post about using 2 DRV8860 together: https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/882856/drv8860-drv8860-ol-fault It looks like you are daisy chaining them correctly.
Regards,
Jacob