This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8881: Working temperature problem about DRV8881PRHRT

Part Number: DRV8881


Hi team,

This device, DRV8881PRHRT, is now used in my customer's nine-inch dome machine. But now the nine-inch dome machine is very hot, so there is a problem that needs your support:

1. Is there anything special about soldering temperature for this IC?

2. What is the maximum allowable operating temperature for this IC and the corresponding operating time?

Regards,

Charlie

  • Hey Charlie, 

    Just curious, how hot is very hot in this case? 

    1. Is there anything special about soldering temperature for this IC?

    Nothing special beyond our PowerPAD layout recommendations, see:

    • PowerPAD Thermally Enhanced Package, SLMA002
    • PowerPAD Made Easy, SLMA004

    The second document has a specific section 3.2 Solder Reflow Profile Suggestion.

    2. What is the maximum allowable operating temperature for this IC and the corresponding operating time?

    Per 6.1 Absolute Maximum Ratings the peak operating junction temperature is 150C.  Max Operating ambient temperature (TA) is 125C per 6.3 Recommended Operating Conditions.  Thermal shutdown temperature is 150C.  

    Regards,

    Jacob