Other Parts Discussed in Thread: DRV10983, USB2ANY, DRV10983EVM
Well TI you went and did it
"Notifier Timed Out
Device GUI.lvlib:GUI Wait for GUI Response via Notifier.vi:5770006:\DRV10983.lvlib:Export Read All.vi\DRV10983 High Level.lvlib:Main.vi"
First what the F, I have spent the best part of 5 hours debugging YOUR unfinished product.
Rant over, what is going on here, this is a brand new out of the box configuration, every step of the process followed to the letter, and still I am getting the above.
I have checked the runtime with LabView blah blah blah, checked voltages, all are nominal but... when I use USB2ANY explorer to enable the i2c line, it does not get pulled high... according to your schematic it should both SDA and SCL as we would expect.
As you may tell I am super p'd with this, it was for a project over Christmas, TI have ruined Christmas...
It is also clear from the MANY other threads this is a common problem, why are you relying on 8 year old runtime files anyway, none of it makes any sense, and I wish I knew this before spending 130€ on this Piece o' crap.
So for the avoidance of doubt, I have installed NI LV Runtime 2014 SP1 32bit, then 64 bit, I have tested ALL of the rail... all good... I am guessing you dont have a rack solution for this, but you must have a KB based on the amount of times this seems to have happened, but I am guessing no scrum behind any of this?!?
"DRV10983 USB2ANY.lvclass:Read Register.vi<ERR>
Register reading not successful!! Please restart the GUI and try again"
Also that looks like a class, not sure if it is being handled in the USB2ANY.dll but it is referenced, also this error comes no matter what chip i pick, this could however just be a generic call to function or class.
I am a little annoyed
Bjorn