This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8912-Q1: Can we connect 12 Solenoid Valves to DRV8912-Q1, which have to be controlled individually?

Part Number: DRV8912-Q1


Hi,

We have a requirement to control 12 solenoid valves at different locations of out Water System. And need your support with interfacing them.

Can we connect 12 Solenoid Valves across the 12 Outputs and GND of the DRV8912-Q1?

Or we can connect only 6 Valves across OUT1 & OUT2, OUT3 & OUT4, OUT5 & OUT6, OUT7 & OUT8, OUT9 & OUT10, OUT11 & OUT12 ?

Awaiting your kind and quick response.

Thank You

  • Vijay,

    The 12 half-bridges in the DRV8912-Q1 can be independently controlled to a HIGH or LOW state via SPI.  Only if you need bi-directional current control would you need to connect across OUT1/OUT2 as this would give you a full-bridge across the 2 half-bridge outputs.

    Regards,

    Ryan