Other Parts Discussed in Thread: DRV8876
Dear, TI support Team.
I want to switch the rotation direction while inputting PWM from the microcontroller to the driver IC in "PWM control mode".
In that case, do I need to connect IN1 and IN2 to the PWM port of the microcontroller respectively?
・In the forward direction, IN2 switches 0/1 → IN2 is PWM
・In the reverse direction, IN1 switches 0/1 → IN1 is PWM
Even if you High-Z (coast) off-duty,
・In the forward direction, IN1 switches 0/1 → IN1 is PWM
・In the reverse direction, IN2 switches 0/1 → IN2 is PWM
We are aware of that, but would like advice if there is a mistake.
Attach the Excel file
DRV8876-Q1 Japanese to English.xlsx
Best Regards,
Hiroaki Yuyama