Other Parts Discussed in Thread: DRV8316-Q1
Meet the requirements of vehicle regulations, three-phase motor driver, working voltage 8~24V, power 3W BLDC motor driver chip which is more suitable?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Meet the requirements of vehicle regulations, three-phase motor driver, working voltage 8~24V, power 3W BLDC motor driver chip which is more suitable?
Hi Xiaofu,
Thank you for posting to the Motor Driver's forum!
The DRV8316-Q1 device, which is AEC-Q100 qualified for automotive applications, is a three-phase integrated FET device with a recommended operating voltage between 4.5V to 35V and a maximum peak output current of 8A. This device also has integrated current sensing and offers the following control interfaces: 3xPWM mode and 6xPWM mode. For more information about this device, please visit the following product page: DRV8316-Q1
Best,
~Alicia