Part Number: DRV8874-Q1
No.1:Function mode switching
Active mode ⇔ sleep mode, switching control
Is it possible to switch modes when PMODE is set to Hi (PWM control mode) and IN1 and IN2 are connected to nSLEEP?
(Normally, the IN1 and IN2 terminals are Lo input, and one terminal is Lo input with his 100% duty during operation.)
Also, if such a control method is adopted, will there be any impact when switching from reverse control or forward control to sleep?
No.2:EN1/IN1,PH/IN2,nSLEEP pins
In the DRV8874Q1 (datasheet), the EN1/IN1, PH/IN2, and nSLEEP pins are pulled down with 100kΩ, but I would like to know the variation in resistance values.
No.3:nFAULT pin
I am considering using the IC with the fault state disabled, will this affect the IC in any way?
If not, is a pull-up resistor necessary?
No.4:IPROPI pin
If the current detection function is not used, is there any problem with OPEN?
No.5:VREF pin
If the IMODE pin is connected to GND and the IPROPI pin is open, is there any problem if the VREF pin is open?
No.6:VREF pin
If the IMODE pin is connected to GND and the IPROPI pin is open, and if the reference voltage must be input to the VREF pin, is there no problem with a 5.0V input?
It is described in the recommended operating conditions (VVREF=0 to 3.6V) in the datasheet, but what is the difference from 5V input?
No.7:Protection circuit
What are the implications of not using the VCP charge pump constant voltage lockout protection?
If not used, is the capacitor between CPH and CPL unnecessary?
No.8:Reverse voltage application
A diode is inserted upstream of the VM pin as a countermeasure against reverse voltage application. Will it affect the IC?
If the IC is not affected, are the above measures sufficient?
(No resistance is inserted between the GND terminal of the IC and the GND of the board.)
If there is any effect on the IC, please tell me the countermeasure against reverse voltage application.