Other Parts Discussed in Thread: DRV8412
Hello team,
We have a project that uses a Piezo motor. When measure the waveform of the driver signal, we found that it consists of 3 signals: clockwise pulse (CW), counter-clockwise pulse (CCW) and COM. Pulse is 300Khz PWM from -60V to 60V reference to COM. When the CW pulse is applied, the CCW must be floated and vice versa.
I have a few questions:
- Can we use DRV8844 to generate the required signal? Will 60V (0.2A) and 300kHz cause to stress the IC?
- Can we use OUT1 as CW signal, OUT3 as CCW signal and OUT2 as COM. To generate CW signal, we will give two 180 degree phase difference pulses to IN1, IN2 and disable OUT3 by EN3 (similar to generate CCW signal). Can that generate a pulse that meets the requirement from -60V to 60V, 300kHz? Will the High-Z state of OUT3 be unaffected?
We hope receive your support,
Best regards,
Danh