Other Parts Discussed in Thread: DRV8706-Q1
Hello,
I am looking into options to fully drive this Peltier element rated at 128.7W, 13.1A, 15.7V (link: https://de.rs-online.com/web/p/peltiermodule/4901402).
Is is possible to use this DRV8145? I want to fully drive the Peltier at 100kHz (or even lower if not possible).
According to the Datasheet, the device is rated at IoutMax = 46A. Does this mean that if I connect two Peltier in series, I can drive both the Peltiers with this driver?
Thank you very much in advance.
Best Regards,