This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8243S-Q1LEVM: Increased VM in fast decay mode

Part Number: DRV8243S-Q1LEVM


Hello team,

My customer is using DRV8243 to drive solenoid. (They are driving the solenoid with H bridge)

However, they are experiencing increase in VM (up to 35V) when fast decay mode.

Is there any ways to reduce the increase in VM?

Would switching between slow decay and fast decay (mixed decay mode) during the brake work?

Best Regards,

Kei Kuwahara