I measure 2.6VDC across the coil of my stepper motor when VM = 24 VDC. Why is the voltage across coil so low eventhough VM is 24 vdc.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I measure 2.6VDC across the coil of my stepper motor when VM = 24 VDC. Why is the voltage across coil so low eventhough VM is 24 vdc.
Hello,
In a stepper motor driver, current is always being regulated using PWM control. As you issue pulses on the STEP input, current will increase or decrease depending on where you are at in the indexer table. Because of the PWM control, you will see lower voltage than VM across the windings.
There are some great videos on stepper motors you can watch below:
https://www.ti.com/video/series/stepper-motors.html
Regards,
Ryan
Thanks Ryan for your reply. I watched the videos on stepper motors as well.
How can I know if my motor is getting enough juice. In order for us to get the required torque, we need 24VDC at 4.1 amps, and I want to make sure the motor is getting the speced power.
Thanks
Ali