Other Parts Discussed in Thread: , MCF8316A
Hi team,
Uses MCT8316AEVM to drive brushless DC motors and operates with adjustable switching power supply (29V supply, approximately 1.3A output current).
After debugging is good, run an aging test, The environment is stable at about 35℃. After about 50 hours of continuous operation, the chip does not work properly and the motor stops. The voltage at the VM and VBAT inputs changes to 4.2 V, while the adjustable switch voltage remains at 29 V, showing an output current of 0.
The original chip of the board was the MCF8316A, which was replaced with the MCT8316A for testing because two chips were burned in succession.
Could you help check this case? Thanks.
Best Regards,
Cherry