Part Number: DRV8461
Hi Dear,
Referring to the evaluation board of DRV8461, it is necessary to monitor the AOUT1/AOUT2/BOUT1/BOUT2/VM voltage,which requires 5 ADC interfaces. as shown in the following figure.
However, the built-in ADC peripheral resources of the microcontroller are insufficient. May I ask if voltage detection can be omitted?

However, the built-in ADC peripheral resources of the microcontroller are insufficient. May I ask if voltage detection can be omitted