Other Parts Discussed in Thread: TPS631000
Hi
In the following graph, the blue signal is the IN1 and the yellow signal is OUT1.
When the solenoid is not connected, the signals are smooth and clean. However, when the solenoid is connected, I get such jittery signal.
Following is the board layout of where the IC is on the board.
I am not able to understand the reason for such behavior. Could it be that the switching of the solenoid is causing interference in the 3V3 signal? Is it also possible for this to cause changes in the input signal?