Hi,
Good Day.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Good Day.
Hello Ray,
We don't have any reference code for the arduino board. The only reference code is the one provided with the BOOST-DRV8711 launchpad which you can find here.
Regards,
Pablo Armet
Hi Pablo,
Good Day. Can you tell me what to do with sleep and reset pins in initialization and throughout the program, because the datasheet doesn't provide much information about those pins? Thank you very much.
Hello Ray,
The nSLEEP needs to be logic HIGH either before or after VM is supplied to the DRV. The RESET pin will reset the internal logic and outputs when pulled logic HIGH. Therefore, RESET pin should be OPEN or tied to GND to ensure the DRV is in active operation.
Regards,
Pablo Armet