This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HAPTICS-CONSOLE: How to increase the the frequency and voltage in Haptic Control Console....

Part Number: HAPTICS-CONSOLE
Other Parts Discussed in Thread: DRV2667EVM-CT, DRV2667

I have DRV2667EVM-CT with me an I'll use it on Haptic control console software  but it has 2000Hz frequency and voltage parameter preinstalled in it. I require 1MHz frequency and 10-120V voltage.

1) It is possible to increase frequency upto 1MHz  and  voltage upto10-120 V. How???

2)Is require any other programing tool or any hardware tool?