Hi
On my eval Board I tried a setup for a customer.
And create a JSON file ( Save -> File)
Now my costomer want to test it.
He ordered a EVAL board.
Setup up alle jumpfes and switches the same.
But the Software says only MOTOR_BREAK.
But break switch is release?!
Tried to download the JSON servera time...
for a short Period it shows MOTOR_RUN the BEAK again.
No Errors or something.
I tried server option with I2C on / off. or Break pin aktiv... no change...
What is the condition to wirte down a saved config
My board is 5 Month old. ( working, top)
The other one is brand new. ( the I2C jumpers where added befor testing...bottom)
I now left my board at customer side. And tried on a other PC... same...
I also tried a new config with download Default config... no change.

I also checked the switches... right one is break?
But sinal is fine 0V or 3.3V.
Any idear?
BR
Andreas