The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8874: current sampling

Part Number: DRV8874
Other Parts Discussed in Thread: DRV8701,

Hi Team,

Q1: Customer used DRV8874. The actual current of the motor is only 60mA, but the read current is 120mA. May I ask what causes it? The same current read by DRV8701 is correct, AIPROPI (μA/A)=450. 

Q2: When sleep is low, the customer uses an oscilloscope to measure OUT1 and OUT2, and there is a 50HZ 12V waveform output directly. May I ask why this happens?

Best regards,

Annie