Part Number: DRV8952
Other Parts Discussed in Thread: DRV8962
Hi team,
Could u kindly help to recommend a device and the requirement is as below:
Vinmax: 45V
Iomax: 10A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zoey,
A device recommendation similar to the DRV8952 that meets those specs is the DRV8962. This device is an integrated driver that offers a operating supply voltage range between 4.5 v - 65 V and can drive up to 10 A with the DDV package.
We also offer gate drivers that can supply higher output current if needed, and can be found in the link below.
Best,
David