This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8145-Q1: DRV8145 as driver for heating foil

Part Number: DRV8145-Q1
Other Parts Discussed in Thread: DRV8144-Q1

Hello,

Can I use the DRV8145 for the purpose of driving this foil rated at 12V 100W?

The driving frequency should be around just 200Hz.

Thanks in advance.

Best,