This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3255-Q1: BLDC motor control

Part Number: DRV3255-Q1
Other Parts Discussed in Thread: DRV8353, CSD19536KCS

Is DRV3255-Q1 gate driver compatible to be used for 2.5 kW motor controller for sinusoidal control with 40 amps continuous current and 62 voltage DC Bus voltage. Is it more feasible to use DRV three phase driver or should I use a half bridge driver for each phase?