This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8834: Recommended motor to combine with this MD?

Part Number: DRV8834

Hi team,

My customer would like to see the performance of this motor driver.

Do we have a recommended motor or a motor you have used and know that it performs okay?

Thanks,

Luke

  • Hi Luke, 

    The motor selection depends on the application and system requirements such as supply voltage, PWM frequency, etc. 

    The DRV8834 is also a DUAL H-bridge motor driver, meaning it can be used for one stepper motor or two BDC motors. Which motor is the customer looking to use?

    Also if possible, please provide system requirements to assist with any possible motor recommendations. Because of the wide variety of motors in the market that vary due to location it is better for the customer to offer a motor suggestion first. 

    The DRV8834 is versatile with its driving capabilities as long as the motor selected fits within the parameters listed on the product page and is run under the recommended operating conditions. 

    Best,

    David