Part Number: DRV8262EVM
I was able to connect once to the DRV8262EVM board. The GUI offered a firmware update. Followed the instructions in the Users Guide and loaded the update. At some point during the update a message appeared about the connection being lost. The update must not have completed successfully. I am now unable to connect to the EVM. The MCU_STATUS blinks at a rate of about once a second. There are no MSP COMxx ports enumerated in the device manager. What is present is an HID device VID_2047&PID_0203 which seems to be an eZ-FET boot loader. Power has been cycled for both the EVM and the PC.
Does the firmware need to be reloaded? If so, what is the procedure?