This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2625: Schematic review

Part Number: DRV2625


Hi Team,

My customer wants to check the schematic of DRV2625 with us, I have checked already with our pinmap and didn't find any problems, could you kindly help double check it? Thank you.

Best Regards,

Remy

  • Hi Remy, 

    I noticed a few things. Firstly, I recommend putting an input capacitor on Vdd. From the datasheet, it is recommended to use a 0.1uF cap with a higher voltage rating than the Vdd. I also do not recommend tying the two regulators together as the device monitors the value. For layout, place both the Vdd and Reg caps close to their respective pin. Also, is NRST connected to a GPIO pin?  

    Regards,
    Sydney Northcutt