This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8251A: Vref value

Part Number: DRV8251A


Is  VREF a logic input?
I understand that the internal impedance is high, and it is not a port where current flows in, but there is no current information or resistance information, so please check it.


Also, is it possible to reduce the out current to zero by setting VREF low (0V)?
In order to protect the microcontroller in the event of an abnormality, it is required to turn off the output by controlling the driver IC. We are planning to achieve this with VREF = 0V, and we want to know.