This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353RS-EVM: LAUNCHPAD-F280025C: Suitable motor

Part Number: DRV8353RS-EVM


Hello sir,

I would like to ask , I have the following (DRV board + Launchpad) which is mentioned above as well.

Can you please recommend the suitable motor for the same, even I have 1000W hub motor and trying to spin it as per user guide upto DMC level-4 but it is not giving us satisfied result so we are getting confused, is it the power supply issue because we are using 30V,30A ps and our motor ratings are 26 poles pair, 48V,10A.

Please recommend the motor which's spices match with DRV83 board.