E2E,
I'm considering to use DRV8245 for the valve controller.
I have 2 questions below.
① Current sense accuracy needs <15% with 1A to 2A.
② How much is the sensing accuracy when over 10.9A?

But if you have alternative device/solution to meet this requirement, please advise me.
I just need H-Bridge driver (not half-bridge), max drive current 30A with high CS accuracy…
Thank you,
Adam