This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMD18200: Test Circuit

Part Number: LMD18200

Hello team,

I have 2 questions about the test circuit in the datasheet.

  1. What is the role of 12Ω resistors connected between pin6 and pin10, & pin7 and pin2? Are they just for test cirucuit, and can I omit them in the real use case?
  2. Why is there 1200uF of capacitor between pin6 and pin7? On the datasheet, it says at least 100uF per Amp of load, so if I am loading with 3A, can I just use 300uF?

       

Best Regards,
Kei Kuwahara