Part Number: DRV8912-Q1
您好,
我用24V电源驱动drv8912芯片,当把nSleep引脚置1以后,nFAULT pin就会报错,当我把EXT_OVP设置为1后,错误就会消失。但是在我设置FLT_CLR位后,状态寄存器IC_STST的OVP位还是1,请问是怎么回事?还有,OVP的阈值只能设置为21V或者33V吗,不能更改为别的值(例如24V)吗?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8912-Q1
您好,
我用24V电源驱动drv8912芯片,当把nSleep引脚置1以后,nFAULT pin就会报错,当我把EXT_OVP设置为1后,错误就会消失。但是在我设置FLT_CLR位后,状态寄存器IC_STST的OVP位还是1,请问是怎么回事?还有,OVP的阈值只能设置为21V或者33V吗,不能更改为别的值(例如24V)吗?


translation:
I use 24V power supply to drive the drv8912 chip. When the nSleep pin is set to 1, the nFAULT pin will report an error. When I set EXT_OVP to 1, the error disappears. But after I set the FLT_CLR bit, the OVP bit of the status register IC_STST is still 1. What's going on? In addition, can the OVP threshold be set only to 21V or 33V? Can't it be changed to another value (such as 24V)?
Hi Annie,
When the nFAULT pin reports an error what is the IC_STAT readout data? Does it show OVP error only? See below the OVP threshold specifications. These are the available options. Based on these specifications for 24V supply you must use EXT_OVP = 1b to avoid triggering an OVP. It cannot be changed to other value.

This selection will detect if the voltage has reached max. specified operating voltage and well within abs max. Typically when a BDC motor is stopped its energy (back EMF) gets pumped to VM node often times increasing the VM voltage from what the power supply is providing. OVP will detect such situations and report is as OVP error. Of course if the power supply exceeds the threshold for some reason that would be detected as well. Thanks.
Regards, Murugavel