Hello,
My customer is trying to figure out how to handle the calibration routine for the DRV2625 for production and is looking for some feedback.
- Could they characterize a number of LRAs and program the average calibration information into their MCU at assembly to use for all production boards? Obviously there is part to part variation with the LRA, but do we think that individualized calibration is needed?
- If you hard code the calibration at assembly, is there an issue with drift or changes in resonance or magnitude over time? Do we think it is okay to do calibration at t=0 and never change these values again? Alternative is running the calibration at every power up where you would capture any changes over lifetime, but this complicates the FW on the device and turn on time.
- They plan to only use haptics as a feedback for touch screen presses on their device, do we think that part to part variation or aging is enough for a user to notice any changes if the calibration values are not ideal?
Thanks in advance!
John