This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8212: MODE pin input current in Sleep mode

Part Number: DRV8212

Hi team,

Let me confirm how we should understand correctly for the imput current on MODE pin in Sleep mode.

We can find the descriptions below on the datasheet.

To ensure lowest supply current draw, TI recommends setting all input pins to logic low to eliminate current draw
through the pulldown resistors in sleep mode. If the MODE pin is set to Hi-Z or logic low, it will not draw current
in sleep mode. However, the MODE pin will draw some current in sleep mode when it is logic high.

Question) Is it correct that the internal pull up/down switches to only 1Mohm pull down in the device? (Is the pullup 75kohm dis-connected in the Sleep mode?)

Thanks in advance.
S.Sawamoto