Part Number: DRV8353RS-EVM
Hello,
I am trying to control a 3 phase bldc motor using the drv8353-evm with in 6x mode. I am using an input voltage of 24V, I can see an output voltage of 34V on the charge pump pin. however, all of the GHx pins are only pulled up to 24V. Can someone help me figure out why this is happening, I have searched on the forums and have not found any answers.
my configuration for the gate driver is
x02: x0080
x03: x0333
x04: x0733
x05: x01e9
x06: x0243