Other Parts Discussed in Thread: DRV8706-Q1, DRV8262, DRV8705-Q1
Hi Team,
The customer tried to short-circuit the two poles of the motor. At this time, the peak current could reach 40A (the designed current limit value is 8A), and the frequency of the peak current was 35KHZ. At this time, the nfault pin was still at high level, and no error was reported to shut down the output.
After replacing different power supplies and batteries, the results are the same.
1. Why is the frequency of peak current 35KHZ?
2. Why is the nfault pin still high after exceeding the hardware current limit?
Current waveform
Schematic diagram
May I ask why this phenomenon occurs?
Regards,
Annie