This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10974: Current limit

Part Number: DRV10974

Hello team,

I want to set current limit to 100mA or 150mA.

On the datasheet, the example values of R(CS) is listed only from 200mA limit.

Can I set the current limit to 100mA or 150mA?
If so, what would be the R(CS ) value? Is there any equation to find the R(CS) value?

Best Regards,
Kei Kuwahara