Part Number: DRV8702-Q1EVM
Other Parts Discussed in Thread: DRV8962, DRV8262
Hi team,
I am testing DRV8702 evm with Eload.. I use PH/EN mode, the duty circle of PWM is 100%. PVDD is 6.2V from buck-boost controller. the load is about 1.14ohm. When driving the load, the device get protected as below waveform. Vtepr is the output voltage of out2. OUT1 is 0V. Is the problem from under voltage protect? Do you have any suggestion to solve this?

Matthew