Part Number: DRV8714H-Q1EVM
Other Parts Discussed in Thread: CSD18512Q5B
Hello Team,
In Fig.2-1 c of Appnote “Current Recirculation and Decay Modes“ (slva321a) the N MOSFET transistors AL and BH are assumed to conduct in reverse mode (source to drain direction) in so-called fast decay mode. I used DRV8714H-Q1EVM and a DC motor in tests. In the CSD18512Q5B external transistors datasheet the only reference to reverse conduction is Fig.9 (Typical Diode Forward Voltage). No other reference justifies reverse conduction.
My questions are:
- can a N MOSFET (enhanced) conduct inverse, from source to drain? If so, why the reverse conduction is not detailed by characteristics like those specific to direct conduction found in the datasheet?
- Why power switches capable of bidirectional current flow are made with two MOSFET transistors connected back-to-back (see slva948.pdf from TI) when a single transistor with both types of conduction would solve the problem?
- I tested a DC brush motor using the DRV8714H-Q1EVM and the DRV87xx EVM GUI. The fast decay mode (transistors AL and BH) is not programmed in either PH/EN or PWM mode. The decay current can follow one of the lower or upper recirculation paths corresponding to the passive or active freewheeling mode. I have attached the oscillogram for synchronous low side decay (forward). Indeed, the transistor Q8 active in recirculation is operated with the voltage VGL1 of approx. 11V. However, the current measured with a current probe does not change in form or value when GL1 is disabled. This fact demonstrates conduction only by freewheeling diodes. How can this fact be explained?

Thanks!
Regards,
Radu