This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8662: Current limit of the boost converter in DRV8662

Part Number: DRV8662

What is the maximum output current of the boost converter in DRV8662? Assuming the inductor is properly selected to handle up to 100 Amps, and the current-limiting resistor is correctly configured, what are the internal limitations of the device itself?

On a related note, I like the functionality of the boost controller in this device. Does T) offer a boost controller chip that can accept a 5V input and boost it to 50V, with an output current of 10-20 mA?