This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8145-Q1: output short vs. load short

Part Number: DRV8145-Q1

TI Team,

in below desciption of OLP, what is the meaning of "output short" and "load short".

How this conditions are defined, and what are diferences between them? 

  • Hi 

    Thank you for your questions.

    -OUTPUT short means "OUTPUT pin is connected to GND(or VM) via low impedance like 0ohm.

    -Load short means, load is normally expected as inductive load like motor. However it become "short" like 0ohm and 0 inductance. Or added 0ohm short parallel with motor load.

    regards

    Shinya Morita