This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8329A: Motor Lock Detection

Guru 12440 points
Part Number: MCT8329A


Hi,

■Question 1: Loss sync times
Loss of sync is one of Motor Lock Detection. When are Loss sync times cleared? For example, when the power is turned on and a command value of a certain rotation speed is input, the motor will rotate, but if the command value is 0 rotations (stopped), will the Loss sync times be cleared? Or does it hold the previous value and accumulate until the power is turned off?

■Question 2: Loss of Sync
Loss of sync is one of the detections of Motor Lock Detection. Am I correct in my understanding that if Loss of sync is disabled, even if Loss of sync is detected, it will not be detected as a motor lock error?

■Question 3: Motor Lock Detection
Is it correct to understand that Motor Lock Detection starts operating after the motor starts from open-loop control to closed control?

Thanks,

Conor