Part Number: DRV8428E
I have some students out here, that for whatever reason, are locked into using the DRV8428E as the motor driver for their project.
( I think they had to submit a BOM, or design specs prior to project completion, and discovered they are having trouble.)
I have read the Data sheet for alternative applications of the DRV8438E/P.
The students have tried connecting the DRV8428E for a stepper motor in a method consistent with the schematic shown in the DATA sheet, on page 26.
and I have verified this. They however have about 8 smoked chips, so i figured it is time to ask for help. The general internet lacks many examples of people using this chip,
So I figured to ask TI.
The project is utilizing an esp32, 3.3VDC, with a separate 12V bus for motor power. Yes, the thermal pad is grounded. Decay is set to GND.
Can some one tell me, or show me, if there is any variation between the DRV8428E stepper motor wiring, and the schematic shown on page 26 of the datasheet utilizing the -P variant:
www.ti.com/.../drv8428e.pdf