Hi,
I have question on this two setup to control a peltier module.
We would like to maintain the temperature of a DUT 40 degree celsius. So for example if the DUT goes above 50 degrees we would like to cool it down to 40 degrees back, if it go to 30 degrees we would like to heat it back to 40 degrees. May I know which are solution are more suitable for my applications? It seem like both of the IC are using PWM input. Can help if there any others reading material on peltier module would be helpful.
thank you and best regards