Part Number: DRV8353RS-EVM
Other Parts Discussed in Thread: DRV8353
Hi,
I'm having some trouble with the gate driver DRV8353RS it is failing after level 2, this is happening during bring-up with no-load of NEMA 17 24V 4000RPM BLDC motors.
1. First we connected the NEMA 17 24V 4000RPM BLDC motors, There is no consistency in motor running sometimes running and sometimes not running, motor was running only at 30V not 24V. Finally ,Resistance estimation is not correct because same 24V tested in Drv8353 EVM board
it was fine and running smooth. But right now the custom board we are facing this kind of issues.
2. During code flashing/debugging, DRV8353RS fault red LED gets suddenly ON and overcurrent faults is 1. Also DRV8353RS IC is getting heated during this condition.
3. Build_LEVEL_1 setup meets as per expectation but Drv8353 chip is continuously failing. Even we tried change the IDRIVE current setting from IDRIVEP_HS = 0.010A to IDRIVEP_HS = 1.000A no change in response and still Drv8353 chip is failing in custom board.
Requesting to you please arrange a call or meeting to discuss in detail.
This is very urgent for us please help.
Regards,
Shambhu Singh
Mobile: - 9763162499